mexico    UK    China
  

Lee Spring
 Lee Spring
Lee Spring
Lee Springs Specialty Parts: Learn About Constant Force Springs
 Lee Spring
Lee Spring

Lee offers Constant Force Springs in four Life Cycle ranges. Each spring is a roll of high yield Type 301 Stainless Steel strip exerting a nearly constant restraining force to resist uncoiling. When the strip is extended, the inherent stress resists the loading force at a nearly constant rate.

Guide to Mounting Constant Force Springs
A Contant Force Spring is usually mounted by first tightly wrapping it on a drum, then attaching the free end to the loading force such as in a counterbalance application. This relationship can also be reversed.

  • The drum diameter should be 10 to 20% larger than its natural diameter.
  • One and one-half wraps should remain on the drum at maximum extension.
  • The strip becomes unstable at long extensions and should be guided to
    prevent twisting or kinking on recoil.
  • Idler pulleys must be larger in diameter than the natural diameter and should never be used to cause back-bending against the natural radius of curvature.



2500 Life Cycle

4000 Life Cycle

13000 Life Cycle

25000 Life Cycle


Return to home page
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
  Phone: 888-SPRINGS (888-777-4647) • Fax: 888.426.6655 • Email: sales@leespring.com            © Copyright 2009 Lee Spring Company